AXIS#.VL.LMJR

Description

This parameter is used in the internal calculation of the current loop acceleration feed forward gain value.

Versions

Action Version Notes
Implemented 02-00-00-000
     

General Information

Type

Read/Write

Units

NA

Range

0 to 100.0

Default Value

0

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.VL.LMJR 0x5011 0xB UDINT 1000:1 - RW False
AXIS2.VL.LMJR 0x5111 0xB UDINT 1000:1 - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen